Browse FAQs

What is the RJ45 pinout for ATV61 / ATV71 drives?

Published date: 26 December 2019

Issue:
Where can I find the RJ45 pinout for ATV61 / ATV71 drives?

Product Line:
All

Environment:
All

Cause:
Can not find documentation

Resolution:
The RJ45 connector uses two wire RS-485 connection for Modbus communications.
Pin 4 is the DB (+). Pin 5 is DA (-). These terminals are for communication.
Pin 7 is 10 VDC and 8 is 0 VDC. These are used to power the remote keypad when connected to this drive or the RS232 to RS485 adaptor when connecting from a PC with Powersuite.
The pins are numbered from Right to Left when looking at the front of the drive.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.