Browse FAQs

In Unity Pro what corrects an 'Inconsistency in Security Databases' error message?

Published date: 29 June 2020


When this error is encountered, do the following:

Is the Security Editor installed?
Yes,
Repair Unity Pro
Make sure the user is logged into the PC with full administrator rights.

No,
Install the security editor, Launch the CD: _security.exe.


Legacy KB System (APS) Data: RESL164292 V1.0, Originally authored by on , Last Edited by on
Related ranges: Unity Pro

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.