Browse FAQs

What are the minimum and maximum cable specifications for Remote I/O ( RIO )?

Published date: 29 June 2020

Maximum drop length is 164 feet.
Minimum drop length is 8.5 feet.
Maximum trunk length is 8400 feet using RG11 and 4600 feet using RG6.
Maximum overall attenuation for the network is 35 db.
Minimum distance between taps is 8.5 feet.
Minimum distance between the RIO head and the self terminating "F" adapter is 18 inches.
Minimum distance between the self terminating "F" adapter and splitter 8.5 feet.



Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.