Browse FAQs

How can I correct a 'Runtime error 339, component dwshk36.ocx or one of its dependencies is not correctly registered or a file is missing' error that is displayed when I try to launch ProWORX 32?

Published date: 26 June 2020

There is a 'repair' function on the Installation CD for ProWORX 32. Performing a 'repair' will usually correct this error.
Note: It can also apply to other .ocx files that are missing.


Legacy KB System (APS) Data: RESL169292 V1.0, Originally authored by on , Last Edited by on
Related ranges: ProWORX

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.