Browse FAQs

How fast can the ConneXium Redundant Ring heal a network failure?

Published date: 09 July 2020

The ConneXium ring managed switch (499NxSx7100 model) sends out proprietary Bridge Protocol Data Unit (BPDU) messages every 20ms as a ring integrity heartbeat. Should a failure be detected, the minimum heal time is 2 BPDU cycles or 40ms for 2 ConneXium switches. Note that additional switches will increase the heal time accordingly due to latency but will range no more than 500ms in a maximum configuration of 50 switches.


Legacy KB System (APS) Data: RESL173814 V1.0, Originally authored by on , Last Edited by on
Related ranges: ConneXium - Ethernet

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.