Browse FAQs

How can I achieve maximum redundancy with my Hot Standby/SCADA system?

Published date: 29 June 2020

To protect against media and Ethernet device failure, consider the following:


1. Redundant Monitor Pro SCADA servers at v7.2 or higher.
2. Mesh Ethernet network using Rapid Spanning Tree protocol on ConneXium 499NxS27100 Ethernet switches
3. Or, ConneXium self-healing Ethernet Ring on the 499NxSx7100 Ethernet switches
4. Redundant Hot Standby PLC's with Quantum 140NOE771x1 modules connected to separate ConneXium switches

Note: Shown are dual Ethernet adapters in the SCADA servers. 2 or more adapters can be bound to a single IP address for adapters that support such a feature. Intel adapters support such a feature known as 'NIC Teaming'.

This will allow for PLC, SCADA server, Ethernet switch, and Ethernet media failure and continue operating.


Legacy KB System (APS) Data: RESL173847 V1.0, Originally authored by on , Last Edited by on
Related ranges: Modicon Quantum

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.