Browse FAQs

Can I use negative values with the ADD 984LL instruction?

Published date: 15 May 2020

This is not possible with the ADD instruction because it supports unsigned decimal format. Consider using the AD16 984LL instruction and power the lower input to the block to specify signed operation.

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.