Browse FAQs

Is there an isolation specification for Quantum point to Quantum bus (backplane)?

Published date: 03 June 2020

Yes there is. The specification " Isolation Input or Output to bus is 1780 Vac for 1 min " This specification is the same for all the Quantum IO modules.


Legacy KB System (APS) Data: RESL180353 V1.0, Originally authored by DaSo on 10/17/2006, Last Edited by DaSo on 10/17/2006
Related ranges: Modicon Quantum

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.