Browse FAQs

What is Remote Area Network ( RAN )

Published date: 26 June 2020

Remote Area Network or RAN was a network method that enabled wireless transfer of data via landline, RS232 serial port, cell phone or satellite connections. The Symax 8030 CRM 560 was a Remote Network Interface Module that used this method of linking IO from field devices to local area and remote area networks. The RAN methodlogy is the basis for transmitting data via radio modems.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.