Browse FAQs

How do you configure a Run/Stop bit in TwidoSuite for a Twido Controller?

Published date: 25 June 2020

Issue:
How to configure a run/stop bit for the Twido controller.

Product line:
All Twido Controllers

Environment:
Twidosoft, Twidosuite

Cause:

To show how to configure a Run/Stop bit for a Twido Controller using TwidoSuite.

Resolution:

To be able to set up a Run/Stop bit in using TwidoSuite you will need to do the following steps.
Open the program and go to program and configure tab.



At this point depending on what controller that you have selected you will have an input that you can configure as a Run/ Stop bit. This will be an input between %I0.0 to %I0.23 depending on the model number. Select the input that you want to be the Run/Stop bit.



Once you have selected and download this into the controller your first input will control your Run/Stop. In this case it will be %I0.0.


Note: the Twido has been obsolete since 2016 and has been replaced with the M221, The M221 has a start/stop switch on the front of every M221.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.