Browse FAQs

How do I setup serial communication between a Twido and a Magelis HMISTU655 using TwidoSuite v2.2?

Published date: 12 June 2020

Goals and Symptoms
This resolution provides a solution for setting serial communication between a Magelis HMISTU655 and a Twido. The RS485 port 1 and port 2 will be used on the Twido to communicate to a HMISTU655 HMI.
Causes and Fixes

Hardware:
TWDLCDA24DRF : Twido Compact PLC
TWDNAC485D: RS 485 connection module for Compact base
HMISTU655: Magelis HMI 3.5"

XBTZ9780 cable: Serial communication cable:
(or XBTZ978 + XBTZN999 adapter)

Software:
TwidoSuite v2.2
Vijeo Designer v5.1
 
1) Setup the Twido Port 1 with the following parameters:
Type: Modbus
Address: 1
Baudrate: 19200
Data Bits: 8 (RTU)
Parity: None
Stop Bits: 1
Response Timeout: 10
Inter-frame delay: 10



Note: Parity must be set to None on Port 1.
 
2) Configure the TWDNAC485 optional port.


 
3) Setup the Twido Port 2 TWDNAC485 with the following parameters:
Type: Modbus
Address: 1
Baudrate: 19200
Data Bits: 8 (RTU)
Parity: None
Stop Bits: 1
Response Timeout: 10
Inter-frame delay: 10



Note: Parity can be set to None or Even on Port 2 using the TWDNAC485D.
 

4) Create the following Ladder section.




This initialize the memory words so that the TWIDO can communication to the HMISTU655. In a real application this may not be required.
 
5) In Vijeo Designer, configure the Modbus RTU serial driver with the following parameters:

Serial Interface: RS485
Transmission Speed: 19200
Retry Count: 2
Parity Bit: None
Stop Bit: 1
Rcv. Time Out: 1 (Sec)
TX Wait Time: 10 (Msec)

 
6) In Vijeo Designer, configure the Modbus EQUIPMENT with the following parameters:

Slave EQUIPMENT Address: 1
Preferred Frame Length: Custom, 120 bytes
IEC61131: 0-based
Word Order: High Word First
ASCII Display: Low byte first

 
7) Create a Integer variable link to %MW10 in Vijeo Designer

 
8) Add a Numeric Display field and configure as shown below:

Attachments
(Removed File URL: 202705_F0B2/HMISTU655.zip)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/7bb4434bde507c20c125774b00109b11/fl_block_5/0.544?OpenElement&FieldElemFormat=gif)(Removed File URL: 202705_F0B2/TWIDO_Magelis.zip)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/7bb4434bde507c20c125774b00109b11/fl_block_5/0.1126?OpenElement&FieldElemFormat=gif)

Legacy KB System (APS) Data: RESL202705 V1.0, Originally authored by MiMe on 06/23/2010, Last Edited by MiMe on 06/23/2010
Related ranges: Twido

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.