Browse FAQs

How does one get a replacement for the Berger Lahr RSM synchronous motor?

Published date: 29 June 2020

Berger Lahr is now Schneider Electric Motion.
Berger Lahr produced many types and models of the RSM synchronous motors.
Some RSM motors are still offered by Schneider Electric while others are no longer produced.
However, it is important to understand that RSM motors are not available in single piece quantities.
All RSM motor types must be purchased in quantities that range from a 15 piece minimum to as many as 25 piece minimum depending on the model.

Therefore in the event you are in need of a single RSM type motor it would be best to contact the builder of the machine in which the RSM motor was installed for a replacement.
Many times the machine builder can provide a spare RSM motor.


Legacy KB System (APS) Data: RESL205110 V1.0, Originally authored by TVe on 04/16/2011, Last Edited by TVe on 04/16/2011
Related ranges: Twin Line SER

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.