Browse FAQs

How to Update and Reload the DTM library in Unity.

Published date: 12 June 2020

Select <Tools> in Unity and then select 'Hardware Catalog' as shown below:


Select the DTM catalog Tab.
The FDT/DTM Catalog window is displayed. Click the <Update> button.



After clicking the <Update button> the progress window is displayed.
The Update has reloaded the catalog.


Legacy KB System (APS) Data: RESL209892 V2.0, Originally authored by BrWa on 12/06/2012, Last Edited by DaSo on 09/06/2013
Related ranges: Unity Pro - SoCollaborative software

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.