Browse FAQs

EcoStructure Control Expert (formerly Unity Pro) error when opening a project. "Can't create LL984 segment. "Impossible due to compatibility. Function list check failed. LL884 language."

Published date: 29 June 2020

 EcoStructure Control Expert  (formerly Unity Pro) versions prior to v7 require a manual install of the LL984 library. The DVD contains a folder
called UnityLL984Library. The zipped file in this folder should be moved to the hard drive, unzipped and the library installed and authorized.


Legacy KB System (APS) Data: RESL212914 V1.0, Originally authored by DaSo on 10/31/2013, Last Edited by DaSo on 10/31/2013
Related ranges: Unity Pro - SoCollaborative software

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.