Browse FAQs

How do I install a MIC file for the Modicon Micro 110CPUxxxxx using Proworx 32?

Published date: 15 May 2020

1. Open the Traffic Cop configuration screen.
2. Using the Rack 1 tab, double click on the desired slot of the backplane.
3. In the Properties window for each slot, choose the appropriate MIC file from the pull down list.

The MIC file matrix is located in the manual on pages 26-27.
The Modicon Micro Ladder Logic Manual can be located at www.modicon.com, click on the search bar and enter 890USE14600.



Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.