Browse FAQs

What is the full ordering part number for the E5600?

Published date: 14 May 2020

Issue
A customer would like to know the full part number of the E5600 for order.

Product Line
E5600 Series

Environment
product ordering

Cause
A customer or end user would like to know the part number for ordering.

Resolution
Part Number Description
E5600020SQD E5600 Socket Meter, Form 2S, Single Phase, Class 200, S Based Meter
E5600090SQD E5600 Socket Meter, Form 9S, 3 Phase, Class 20, S Based Meter
E5600120SQD E5600 Socket Meter, Form 12S, 3 Phase, Class 200, S Based Meter
E5600160SQD E5600 Socket Meter, Form 16S, 3 Phase, Class 200, S Based Meter
E5600360SQD E5600 Socket Meter, Form 36S, 3 Phase, Class 20, S Based Meter
E5600450SQD E5600 Socket Meter, Form 45S, 3 Phase, Class 20, S Based Meter



Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.