Browse FAQs

Is it possible to communicate to a Sepam relay with SFT2841 via an ION7550/ION7650 meter?

Published date: 14 May 2020

Issue   
Customer would like to configure a Sepam via an ION meter over a network.

Product Line    
SFT2841

Environment   
Communication using SFT2841 over the network 

Resolution   
SFT2841 only works with port 502 for setting up a network connection.  The ION meters don't use port 502 for external softwares to communicate.  The only way one will be able to setup the network connection for SFT2841 is to use a gateway that supports port 502.  


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.