Browse FAQs

Does the SEPAM Series 20, 40, and 80 protection relay save Waveform Captures (WFC) in binary or ASCII Comtrade format?

Published date: 14 May 2020

Product Line
SEPAM Series 20, 40, 80 relays

Environment
SEPAM Relays
SFT2841


Cause
Customer is saving the SEPAM relay WFC and would like to know the format.
 
Resolution
When a new SEPAM fault recording (waveform capture, WFC) is uploaded using SFT2841 two separate files are stored. The WFC data file (xxx.dat) is stored in binary and contains all of the data points that make up the waveform. The WFC configuration file is stored in ASCII (xxx.cfg) and provides the configuration of the plot.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.