Browse FAQs

Cannot Save Files Located on the ION Enterprise Primary Server from a Secondary Server or Client installation

Published date: 27 May 2020

Goals and Symptoms

When you install ION Enterprise on a machine running Windows 2003 Server, the new default permissions settings prevent users from saving files from a secondary server or client installation.  Users receive an error message when they try to save a files on the primary server from different machines.

Facts and Changes

Keywords

Windows 2003 Server

ION Enterprise

Vista diagrams

File permission

Read Only

Causes and Fixes

See attached.

Attachments

(Removed File URL: 179466_C77A/Cannot_Save_Files_Located_on_a_Primary_Server_From_a_Secondary_Server_or_Client_Installation.pdf)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/e70c7b831c61db6dc12571db00837a65/fl_block_5/0.5F8?OpenElement&FieldElemFormat=gif)


Legacy KB System (APS) Data: RESL179466 V2.0, Originally authored by DaMi on 08/30/2006, Last Edited by DaMi on 09/01/2006
Related ranges: ION Enterprise

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.