Browse FAQs

What does it mean when the Power Server status light is blinking red?

Published date: 27 May 2020

 

It means that there is an internal problem with the Power Server. The Power Server must be returned via RMA. text
Version: Version 3.1 and above. text

Legacy KB System (APS) Data: RESL179484 V1.0, Originally authored by DaMi on 08/30/2006, Last Edited by DaMi on 08/30/2006
Related ranges: PowerServer

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.