Browse FAQs

Will the ION 8800 device support higher Ethernet speed than 10Base-T?

Published date: 14 May 2020

Product Line   
ION8800

Resolution
All Ethernet capable ION meters (ION 73XX, 75XX, 76XX, 7700, 8XXX) support only 10Base-T half-duplex Ethernet. There are no plans to increase the speed capability of the network interface card on any ION devices at this time (Feb 15, 2006). According to the hardware R&D team, making our meters full duplex won't increase performance as there are only so many CPU cycles available to process the ethernet data anyway.

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.