Browse FAQs

How to clear and disable all CM3000/4000s data log files?

Published date: 27 May 2020

Issue
Customer would like to clear and disable data logs.

Product Line
CM3000
CM4000


Environment
Factory Reset Data Logs

Resolution
*Warning: All custom logs will be lost.*
Clears all data log files (data and configuration).

  1. Write 32 to register 8001
  2. Write 1120 to register 8000

To write to a register from a computer download Modbus tester from FA180037. Once Modbus Tester is open:

  1. Enter the IP address related to the meter.
  2. Enter the Slave ID (the Com ports unit ID).
  3. Enter 8000 as your Starting Register.
  4. Enter 2 for # of Registers
  5. Click Read.
  6. Enter 1120 in the box to the right of 408000.
  7. Enter 32 in the box to the right of 408001.
  8. Click Write.
To write from the front display:
  1. From the Front Panel Main Menu, select Diagnostics
  2. Select Read/Write Regs. The password prompt displays.
  3. Select your password. The default password is 0.
  4. The Read/Write Registers Screen displays.
  5. Scroll through the register numbers with the arrow buttons
  6. Write 32 to register 8001 by pressing the enter button on register 8001.
    1. The Hex and Dec values begin to blink.
    2. Use the arrow buttons to scroll through the numeric values.
    3. Set the register to 32.
  7. Write 1120 to register 8000 by pressing the enter button on register 8000.
    1. The Hex and Dec values begin to blink.
    2. Use the arrow buttons to scroll through the numeric values.
    3. Set the register to 1120.
  8. Press the menu button to save the changes.
*Reference CM3000 Register List Commands Page (Page 314).
*Reference CM4000 Register List Commands Page (Page 359).

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.