Browse FAQs

Advanced Reports error when creating Usage Reports: [ERR_16]Error publishing report (NAME) cannot be created under the given folder (number) because it must be under folder number 23 either directly or indirectly.

Published date: 14 May 2020

Issue
Below is a screen capture of the actual error:


Product Line   
AR

Resolution

The folder or folders that Advanced Reports is attempting to save to, does not exist.

1. Go to the Admin tab and select Crystal Management Console.
2. Log in using Administrator as username and leave the password section blank.
3. Browse to Folders and follow the hierarchy below and create the folders and sub-folders as they appear with the same names and capitalization.

.

4. Double check the PowerLogic Reports folder rights as well


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.