Browse FAQs

Can not preview or print PowerLogic System Reports in System Manager Software (SMS) when clicking on the preview button. Nothing happens!

Published date: 15 May 2020

Product Line           
SMS 4.x
SMS 3.x

Resolution
This behavior occurs when there is no default printer set up on the machine attempting to run the System Report. To resolve this issue add any printer or printer driver. The printer does not have to be physically connected.
 


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.