Browse FAQs

Web Page Generator (WPG) v 3.5 reset function requires Java.

Published date: 15 May 2020

Product Line
Web Page Generator

Environment
Web Page Reset

Resolution
The reset function of WebPageGenerator (WPG) web pages requires the use of MS JVM except for Compact NSX that works in both MS and SUN Java Virtual Machine. A user can select JVM using IE, as shown below, by selecting the gear in the top right of the browsing window and selecting internet options from the drop down menu. In this case, SUN JRE v1.60 is used to run the applet. If Java (Sun) is unchecked, MS JVM will be used.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.