Browse FAQs

Can an ECC21 send E-mails generated from alarms of downstream devices?

Published date: 15 May 2020

Issue
An ECC21 device is connected to a serial network. The customer wants downstream alarms to be included in the ECC21's email alerts.


Product Line      
ECC21


Environment
ECC21 enabled device on a serial network


Resolution
It is not possible to set up email alerts for devices downstream of an ECC21.
The ECC21 can only email alarms from the device it is inserted, does not read data from downstream devices.

 


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.