Browse FAQs

What user name and password do you enter for the Credential User Name and Password fields in the Relay and Recipient Configuration page of Active Pager Module (APM) v6.0 and v6.1?

Published date: 15 May 2020

Product Line 
APM 6.x

Resolution
The credential user name and password fields are only necessary to fill out if the SMTP server is setup to require a user name and password. Not all SMTP servers are setup to require the use of a user name and password to send messages. If a user name and password are not needed, you can either leave these fields blank or enter anything into them.

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.