Browse FAQs

Can a PM8G work with a Power Meter 710 (PM710) or Power Meter 750 (PM750)?

Published date: 19 May 2020

Product Line
PM700
PM750
PM800

Resolution
No, the PM8G that is used for a metal gasket retrofit for a PM800 Series can not be used for the PM700 Series.
The PM700 Series doesn't have the rounded groove like the PM800 series does for the remote or integrated displays. The only way the PM700 series can be mounted is by using a 3.62 inch by 3.62 inch cutout. For more information refer to the PM700 Installation Manual.
Thus, a PM700 Series cannot replace a traditional analog meter.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.