Browse FAQs

What is the minimum distance between Modbus Plus taps?

Published date: 08 July 2020

Issue:
Minimum distance between the Modbus Plus taps 990NAA23000

Product line:
Modbus Plus

Cause:
Communications issues with shorter cable lengths.

Resolution:
For the Modbus Plus taps the minimum distance between nodes is ten feet, 10ft. The length of the drop from the tap is included, the formula is (one drop length + second drop length + distance between taps) must be greater than 10 feet. If the drops are long enough there is no minimum distance between taps.



Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.