Browse FAQs

Which cable do I need to connect an XBTG2110 to an Micrologix PLC using DF1 protocol

Published date: 14 May 2020


XBTZ9731 Cable
XBTZG999 Adapter

The XBTZG999 adapter connects to the DB25 COM port # 1 on the XBTG2110. The XBTZ9731 cable connect to the XBTZG999 adapter to the MiniDin of the Micrologix PLC.



Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.