Browse FAQs

How many optional modules does the Power Meter 800 Series (PM800) support?

Published date: 19 May 2020

Issue
How many optional modules does the Power Meter 800 Series (PM800) support?

Product Line
PM800 series meter

Cause
Customer would like to know the maximum number of modules PM800 series meter can support.

Environment
Installing maximum number of modules on PM800 series meter.

Resolution
In March of 2005 a redesigned power supply changed the limits of how many option modules were allowed and the de-rating levels for operating temperature.
The series 800 Power Meter supports up to two (2) option modules. There are couple different ways this can be done.

1) One I/O module (ex. PM8M2222) and PM8ECC
2) Two I/O modules (ex. PM8M2222) are mounted together with control power over 370 Vac and the operating temperature rating must be reduced to -25° to 50°C. The operating temperature rating is -25°C to 70°C when the control power is < 370 Vac.

NOTE: Keep in mind that the PM8ECC can be installed only on any Series 800 Power Meter that was manufactured after March 2005. 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.