Browse FAQs

MSA141 Analog Output Module Installation Sheet, Instruction Bulletin (ANSI), 63230-216-253A1, May 2007

Published date: 19 May 2020

The MSA141 module converts one of the Sepam measurements into an analog signal. Measurement selection is determined by parameter setting:
0-10 mA, 4-20 mA, or 0-20 mA analog signal according to parameter setting.
To scale the analog signal, set minimum and maximum values of the converted measurement.
Examplethe setting used to set phase current (Ia) as a 0-10 mA analog output with a dynamic range of 0-300 A is: minimum value = 0 maximum value = 300 (3000 .. 0.1A = 300.0 A)
Any one of the CCA770 (2 ft or 0.6 m), CCA772 (6.6 ft or 2 m) or CCA774 cables (13.1 ft or 4 m) connects a single module for each Sepam base unit.

see attachment
63230-216-253_A1_MSA141_Install Sheet.pdf

 


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.