Browse FAQs

ACE937 Fiber Optic Interface Installation Sheet Instruction Bulletin (ANSI), 63230-216-257A1, June 2007

Published date: 19 May 2020

The ACE937 fiber optic interface is used to connect the Sepam relay to a
fiber optic communication star system. This remote module is connected to
the Sepam base unit by means of a CCA612 cable.


See attachment for details.

63230-216-257A1_ACE937_Install Sheet.pdf

 


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.