Browse FAQs

Wiring a 2-wire Transmitter to an STBACI1400 Analog Input

Published date: 04 June 2020

Issue
This resolution describes how to wire 2-wire analog transmitters to the inputs of an STBACI1400 analog input module.


Product Line
Advantys STB
   STBACI1400


Resolution
2-wire analog transmitters require a loop power supply to power the loop. The following diagram describes how this is done with a single power supply for all loops.


Legacy KB System (APS) Data: RESL192944 V1.0, Originally authored by DaDz on 10/08/2008, Last Edited by DaDz on 10/08/2008
Related ranges: Advantys STB

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.