Browse FAQs

Can the Multi Circuit Meter (MCM) monitor 3-wire and 4-wire loads at the same time?

Published date: 19 May 2020

Issue
Is the MCM able to monitor 3-Wire and 4-wire loads at the same time

Environment
System Type
Multi Circuit Metering


Resolution
The MCM can monitor 3-Wire and 4-Wire loads but the voltage source must be the same 4-Wire source.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.