Browse FAQs

What database connection settings should be used in the Sequence of Events Recorder (SER) 7.0 or 7.1 Migration Utility?

Published date: 20 May 2020

Issue

User needs to connect to the Sequence of Events Recorder Software (SER) database to import, export, or migrate data using the Migration Utility.

Enviroment

SER version 7.0 & 7.1

Migration Utility Settings

Server: .\POWERLOGICES
Database: PLES_SER
User: sa
*Password: Pa55w0rd


*Note: that the password contains a zero and not the letter O.

 


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.