Browse FAQs

System Manager Software (SMS) v 4.x install shield error setup.dll.cpp

Published date: 20 May 2020

Issue
When installing System Manager Software (SMS) the following error occurs when starting InstallShield Wizard.
"SetupDLL\SetupDLL.cpp (469)
pAPP:
PVENDOR:
PGUID:



Solution
The System Environment Variable is set with the Temp Directory to C:\Temp, but this directory does not exist. Create the "Temp" folder on the local drive and the installation will run.
The System Enviroment Variable configuration is located under My Computer > Properties > Advanced settings.

This applies to: SMS version 4.0x, and 4.2.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.