Browse FAQs

Not able to display Real Time Trend Reports in System Manager Software (SMSPE) Web client.

Published date: 14 May 2020

Product Line:  
SMS Web Client
 

Resolution:  

Follow the steps below for one solution:  

1. Verify that the PLTrend.dll virtual directory exist in IIS.
2. Right click on the PLTrend.dll directory.
3. Click on the Configuration Button.


4. Then select the application extension ".trend".
5. Click Edit.



6. Uncheck the box "Verify that file exists".


7. Perform an IIS reset and the issue should be resolved


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.