Browse FAQs

Can the stop bits communication value be changed on an Ethernet Gateway EGX100, EGX150, EGX200, or EGX400 to match the stop bits value on a third party device?

Published date: 14 May 2020

Product Line:  
Ethernet Gateways EGX100, EGX150, EGX200 and EGX400

Resolution:  
If a third party device uses a different communications stop bit value other than the EGX's default then set the EGX's parity to none. The devices should then be able to communicate.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.