Browse FAQs

Can the ribbon cable for the Branch Circuit Monitor (BCM) be extended with a male-to-male connector and a second ribbon cable?

Published date: 14 May 2020

Product Line:  
BCM

Resolution:  
The ribbon cable can be extended up to 20 feet maximum. Two cables cab be connected together using a male-to-male pin connector. It is best to use a solid ribbon cable when possible and keep the cable as short as possible. Any extra connections used can create noise and distortion which can decrease accuracy.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.