Browse FAQs

Can Event Notification Module (ENM) or Active Pager Module (APM) be used to send text messages to cell phones?

Published date: 09 June 2020

Issue
User would like to receive text messages via APM or ENM

Product line
Active Page Module (APM) 5.x, 6.x
Event Notification Module (ENM) 7.x, 8.x

Environment
SMS Text Message option

Resolution
Active Pager Module (APM) or Event Notification Module (ENM) allows SMS text messaging functionality. All major US and Canada cellular carriers will accept emails addressed to cell phone numbers, convert the email to an SMS text message, and forward it to the specific wireless number. SMS text messaging is limited to 160 characters. 

Use the EMAIL option in the Delivery Relays and follow the specific format of 10DigitNumber@cell.carrier_domain.com to send the pages to a cell phone. The following chart lists the domains for each of the major carriers.

Alltel: @message.alltel.com 
Cingular/AT&T: @txt.att.net 
Nextel: @messaging.nextel.com 
Sprint: @messaging.sprintpcs.com 
SunCom: @tms.suncom.com 
T-mobile: @tmomail.net 
VoiceStream: @voicestream.net 
Verizon: @vtext.com
U.S. Cellular: @email.uscc.net

Bell: @txt.bell.ca
C Spire: @cspire1.com
Eastlink: @txt.eastlink.ca
Fido: @fido.ca
Koodo Mobile: @msg.koodomobile.com
MTS: @text.mtsmobility.com
PC Mobile: @mobiletxt.ca
Public Mobile: @msg.telus.com
Rogers: @pcs.rogers.com
Sasktel: @sms.sasktel.com
Solo Mobile: @txt.bell.ca
TBayTel: @pcs.rogers.com
TELUS: @msg.telus.com
Virgin Mobile: @vmobile.ca
WIND Mobile: @txt.windmobile.ca

For example, if your cell number is 555.666.4455 and you have sprint service, you would choose Email as the Delivery Relay and enter the following in the "To" Section:
5556664455@messaging.sprintpcs.com 

Note: The user would still use their existing SMTP server information for sending email messages as text messages.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.