Browse FAQs

The Logging Box under device logging for EGX400 is greyed out

Published date: 09 June 2020

Issue:

The check box that enables logging for any device in the device logging page of an EGX400 is greyed out.



Product Line:
EGX400

Environment:
EGX400 Onboard Data Logging

Resolution:

Verify under device list that the Device Type is correctly set for the device. Selecting modbus or powerlogic as device type when device has its own device type will disable logging for that device and the logging box will be greyed out.



Once the device type is correctly setup, the logging box will work.



 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.