Browse FAQs

What Wiser device should be used to control and monitor a water heater?

Published date: 22 June 2020

Issue:
Help with product selection for a Wiser device to control a water heater

Product Line:
Wiser Home Management System (EER series USA model only)

Environment:
a residential home or small commerical facility

Cause:
Product selection question

Resolution:
Depending on the situation, water heater contol could be done with one of 4 Devices:  Large Load Controller (EER260LLCR),  30 Amp Load Control Relay (EER42200), 5 Amp Load Control Relay (EER42300), or 15 Amp Smart Plug (EER40200 or EER41200)
 
For a water heater with a gas burner heating element, the electrical controls circuit will not draw much power.  It the control circuit is shut off, then the water heater will be shut down.  A 5 Amp Load Control Relay could be used.   If the controls connect directly into a 120V wall receptacle via a standard plug, the Wiser Smart Plug would be a good option.  

For a 120 volt electric heater, the Wiser 30 Amp Load Control Relay would be the best option.  

For a 240 volt electric water heater, the Wiser Large Load Controller is the recommended device.   The Large Load Controller is the only Wiser deviced capable of switching a 240V ciruit.   2 pole breakers are available for the large load controller in 20,30,40,50, and 60 amps.  If power monitoring is desired with the Large Load Controller, then the Current Transformers (EER260LLCCT1, EER260LLCCT2) will have to be ordered seperately. 
 

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.