Browse FAQs

What is the part number for the Modbus-to-Ethernet Gateway for the Altivar Drives and Altistart Soft Starters?

Published date: 15 June 2020

Issue:
Looking for the Modbus-to-Ethernet Gateway part number.

Product Line:
All

Environment:
All

Cause:
The drive or Soft Starter has built in Modbus communication. A gateway is needed in order to interface with Ethernet TCP/IP
 

Resolution:
The EGX100SD will allow interfacing between Modbus and Ethernet TCP/IP. The product Data Sheet is attached. 
 


 


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.