Browse FAQs

Where can I find more information on the 9001 30mm operators?

Published date: 24 June 2020

Issue:
9001K/SK/KX additional specification and rating information.

Product Line:
Push Buttons and Operator Interface

Environment:
All 9001K/SK/KX product

Cause:
Customers are unsure where to find specification and rating information if it is not in Digest 176

Resolution:
Additional information about ratings and specifications can be found in Harmony 9001K/SK/KX 30mm Pushbutton catalog which can be downloaded here:  http://download.schneider-electric.com/files?p_Doc_Ref=9001CT1103


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.