Browse FAQs

Can you order a enclosed NEMA 3R rated variable speed drive over 100HP?

Published date: 22 June 2020

Issue:
125 hp drive in a NEMA 3R enclosure is desired

Product Line:
Enclosed Field drive ATV61 and ATV71,

Environment:
8930 IFD Field Drives

Cause:
None

Resolution:
The Field Drive can be acquired in a NEMA 3R enclosure per the following specifications:
Altivar 61 drive: Type 3R rating at 230 V (1-125 HP) and 460 V (1-700 HP) (higher HP also attainable)
Altivar 71 drive: Type 3R rating at 230 V (1-100 HP) and 460 V (1-600 HP) (higher HP also attainable)

See IFD manual 30072-454-01
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.