Browse FAQs

Does the E5600 socket meter support a Delta Configuration?

Published date: 16 June 2020

The 12S socket base is the only base that supports 3 phase 3 wire delta configuration. The 12S socket base does not support current transformers. The 45S socket base is intended for a 4 wire delta with a center tapped leg.
The E5600 meter supports the following forms and system type below.
Also attached is a wiring of each socket. 

Note*: Current transformers can only be used with the class 20 forms. For more information on the current transformers, look to resolution FA212300. 

Product Line: E5600

Keywords: Delta, E5600, 3-wire


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.