Browse FAQs

What software is used to program the Berger Lahr WDP5-118?

Published date: 29 June 2020

The software used for programming the Berger Lahr WDP5-118 is Bpro/PC1 software.
The software is available in the Zip file which is attached to this FAQ

In order to connect to the WDP5-118 you must have an RS485 communication adapter.

it should be noted that support of WDP5 products has been discontinued as for these products are obsolete and no longer available.

Rev 10-23-18

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.