Browse FAQs

May the PM8RD be connected to the EM4800 meter?

Published date: 17 June 2020

Issue:
May the PM8RD be connected to the EM4800 meter?

Product Line:
EM4800, PM8RD

Cause:
It may be difficult for the customer to navigate through the display on EM4800 meter.

Resolution:
Therefore, recommendation for customer is to use remote display from PM8 which is supported On EM4800 meter. The customer would need to purchase the PM8RD which comes with the 12’ RJ 11 cable that plugs into the remote display port on the EM4800 meter. This allows customers to have better capability to look at their values and configure the meter.
 


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.