Browse FAQs

EM4800 FTP logging setup

Published date: 23 June 2020

Title
EM4800 FTP logging setup

Issue
Procedure to setup a FTP site for the EM4800 series meter to upload logging data.

Product Line
EM4800 series meter

Environment
FTP site
Windows 7/ Server 2008 

Cause
Access onboard logging files using FTP.

Resolution
The EM4800 series multi circuit meter can be configured to automatically upload onboard logging to a server by setting up a FTP site on the server. 

Attached below is a step by step guide on configuring the FTP site on the server and configuration changes required to be made for the meter.

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.